The devices have four built-in tamper responses that can be triggered from the FPGA Fabric. The Tamper macro, exposes these tamper response inputs to the FPGA fabric. The tamper responses are initiated by the System Controller after receiving a tamper event described in the Tamper Detection Flags section, but they may also be initiated on-demand by the user (for example, if the users have their own system level tamper detection connected to FPGA IOs).
Tamper responses are initiated through dedicated control wires from the fabric to the System Controller.