To display information about the programming commands available in the MDB, type
help [programming option]
. The following table provides additional
information for these commands.
set
command, including the tool property options, must be executed
before the Hwtool
command is issued, otherwise the changes to the tool
properties will be ignored.Command | Description |
---|---|
Program | Programs device memory with the image specified by the file. Note: If
the path or filename has spaces in it, you must use the quotation
marks. If there are no spaces in the path of filename, the quotation
marks are not needed, as shown below.
Command format:
|
Upload | Uploads the executable image to MDB memory. The source of the instructions to be loaded is the contents of the memory of an attached PIC® device through the programmer or debugger. Command format:
|
Dump | Writes the device memory to a hex file. Command format:
The
The |