The Oscilloscope trigger sub-module helps to identify and lock on to only the portion of the input signal desired. Depending on the operating mode set by the run controls, the trigger can:
Lock on to a periodic signal and constantly update the plot
Only update the plot when the signal exceeds some level
The edge triggering mechanism is looking for the signal to cross the trigger level. For a positive edge trigger, the signal must go from below the trigger level, to above the trigger level.
The trigger mechanism has two edge trigger modes: Positive and Negative Edge Trigger.
The trigger level can be adjusted in three different ways:
Enter a trigger level value into the text box. Press the TAB keyboard button or click the mouse outside the text box to let the new value take effect.
Click on the up/down arrows located to the right of the text box
With the mouse cursor positioned over the text box, scroll the mouse wheel to increase/decrease the trigger level setting
Drag the trigger level line in the plot area to a new position
The Oscilloscope trigger sub-module uses one of the channel signals when looking for the trigger condition.
Click the colored Trigger source button corresponding to the channel chosen for use as a trigger source. The active Trigger source button will be highlighted.