36.5.9 ASI System Status

Name: ASI_SYS_STATUS
Offset: 0x0B
Reset: 0x01
Property: -

Bit 76543210 
 BDEFERASEFAILSYSRSTINSLEEPPROGSTARTUROWSTART BOOTDONELOCKSTATUS 
Access RRRRRRRR 
Reset 00000001 

Bit 7 – BDEF Boot Sequence Done or Chip Erase Failed

This bit is set to ‘1’ if the chip erase has failed (ERASEFAIL bit is ‘1’) or the boot sequence is complete (BOOTDONE bit is ‘1’).

Bit 6 – ERASEFAIL Chip Erase Key Failed

This bit is set to ‘1’ if the chip erase has failed. This bit is set to ‘0’ on Reset. A Reset held from the ASI Reset Request (ASI_RESET_REQ) register will also affect this bit.

Bit 5 – SYSRST System Reset Active

When this bit is set to ‘1’, there is an active Reset on the system domain. When this bit is set to ‘0’, the system is not in the Reset state.

This bit is set to ‘0’ on read.

A Reset held from the ASI_RESET_REQ register will also affect this bit.

Bit 4 – INSLEEP System Domain in Sleep

When this bit is set to ‘1’, the system domain is in Idle or deeper sleep mode. When this bit is set to ‘0’, the system is not in any sleep mode.

Bit 3 – PROGSTART Start NVM Programming

When this bit is set to ‘1’, NVM programming can start from the UPDI.

When the UPDI is done, the system must be reset through the ASI Reset Request (ASI_RESET_REQ) register.

Bit 2 – UROWSTART  Start User Row Programming

When this bit is set to ‘1’, user row programming can start from the UPDI.

When the User Row data have been written to the RAM, the UROWDONE bit in the ASI_SYS_CTRLA register must be written.

Bit 1 – BOOTDONE Boot Sequence Done

This bit is set to ‘1’ when the CPU is done with the boot sequence. The UPDI will not have access to the ACC layer until this bit is set to ‘1’.

Check also that SYSRST is ‘0’ before proceeding.

Bit 0 – LOCKSTATUS NVM Lock Status

When this bit is set to ‘1’, the device is locked. If a chip erase is done, and the lock bits are set to ‘0’, this bit will be read as ‘0’.