1.1.4 PIC32CZ CA80 Curiosity Ultra Development Board: Building and Running the CAN Bootloader Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions.

Path of the application within the repository is apps/can_bootloader/.

To build the application, refer to the following table and open the project using its IDE.

Setting Up PIC32CZ CA80 Curiosity Ultra Development Board

  • PIC32CZ CA80 Curiosity Ultra Development Board is used for both Host development kit and Target development kit
  • Connect PIC32CZ CA80 Curiosity Ultra development board to another PIC32CZ CA80 Curiosity Ultra development board as per the pin connections shown below
    PIC32CZ CA80 Curiosity Ultra Development Board - 1PIC32CZ CA80 Curiosity Ultra Development Board - 2
    CANH, CAN3CANH, CAN3
    CANL, CAN3CANL, CAN3
    GND, CAN3GND, CAN3
  • Connect the Debug USB port on the board to the computer using a micro USB cable

Building and Configuring CAN Host Applications

Using CAN NVM Host Application to Send the Application Binary to Target Development Kit

If the NVM Host development kit being used is other than PIC32CZ CA80 Curiosity Ultra Development Board then follow the steps mentioned in Configuring NVM Host Application Project.

  1. Open the NVM host application project host_app_nvm/firmware/pic32cz_ca80_curiosity_ultra.X in the IDE.
    • If a NVM host application project of different development kit is used then open that project in the IDE
  2. Build and program the NVM host application using the IDE on to the Host development kit.
    • The prebuilt test application image available under host_app_nvm/firmware/src/test_app_images/image_pattern_hex_pic32cz_ca80_cult.h will be programmed on to the Target development kit with default host_app_nvm project configuration
  3. Jump to Running the Application.

Running the Application

  1. Open the bootloader project bootloader/firmware/pic32cz_ca80_curiosity_ultra.X in the IDE.
  2. Build and program the application using the IDE on to the Target development kit.
    • LED1 will be turned-on to indicate that bootloader code is running on the target
    • LED1 will turn on when the bootloader does not find a valid application; i.e., the first word of the application (stack pointer), contains 0xFFFFFFFF
  3. If the test application is being programmed, open the Terminal application (e.g., Tera Term) on the computer and configure the serial port settings for Target development kit as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  4. Press the Switch SW1 on the Host development kit to trigger programming of the application binary.
  5. Once the programming is complete:
    • LED1 on the Host development kit will be turned on indicating success
    • The Target development kit will be reset. Upon re-start, the bootloader will jump to the user application.
    • If the test application is programmed then LED1 should start blinking and the user should see below output on the Target development kit console
  6. Press and hold the Switch SW1 to trigger Bootloader from test application and the user should see below output.
  7. Press Reset button on the Host development kit to reprogram the application binary.
  8. Repeat Steps 4-5 once.
    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 6