9 Configuring Internal Pull-ups on Default I2C pins
Newer device families feature dedicated I2C pads that provide the ability to reconfigure certain GPIO characteristics to better meet the I/O requirements of I2C communication. The weak pull-ups on standard GPIO pins are typically not strong enough to be used on the I2C bus and instead external pull-up resistors of the appropriate values are typically incorporated into the design. The I2C specific pads allow users to program the weak pull-ups on those pins to allow either twice or ten times the standard weak pull-up current for a GPIO. In many applications, these stronger internal pull-ups can sufficiently drive the I2C bus and can be used in place of external pull-up resistors.
| PU[1:0] | I2C Pull-up Selection Bits | Internal Pull-up Value (RPU) |
|---|---|---|
11 | Reserved | Reserved |
10 | 10x Current of Standard Weak Pull-up | |
01 | 2x Current of Standard Weak Pull-up | |
00 | Standard GPIO Weak Pull-up |
The internal pull-ups on I2C dedicated pads can be controlled by writing to the PU[1:0] bits of the I2C pad Rxy Control (RxyI2C) register. In order to use the PU[1:0] bits for internal pull-up selection, weak pull-ups must be enabled by setting the corresponding WPUx bits. Once weak pull-ups have been enabled on the I2C dedicated pins being used for SDL and SCL, they will default to the standard GPIO weak pull-up strength. If the user wishes to use the internal pull-ups as opposed to external pull-ups on the bus, the PU[1:0] bits would need to be set accordingly to adjust the strength of the internal pull-ups to either twice or ten times the current.