11 UART Module with Protocol Support – Setting up a DMX Receiver
The UART module with protocol support can be configured as a DMX receiver and includes the built-in hardware support to automatically detect and respond to a valid Break condition. The UART with protocol module features a configurable address range, in which the module will ignore all the data bytes outside of the specified range in a DMX packet. In addition to the configurable address range, the module can also be setup to wait for and verify the reception of two Stop bits at the end of a DMX packet by setting the STP[1:0] bits of the UxCON2 register accordingly.
The start address of the configurable address range can be specified by writing to the UART Parameter 2 (UxP2) register and the end address can be set using the UART Parameter 3 (UxP3) register. The UART module only needs to be configured once as a DMX receiver and does not need to be updated for every DMX packet, unless the address range has changed. Example 11-1 demonstrates how a device that has this UART module can be configured as a DMX Receiver. The key configuration settings needed to configure the UART module as a DMX Receiver are:
- MODE[3:0] =
1010- selects the DMX mode - TXEN =
0- disables the transmitter - RXEN =
1- enables the receiver - RXPOL =
0- selects regular polarity - STP[1:0] =
10for verifying the reception of two Stop bits - UxP2 = address of first byte to receive
- UxP3 = address of last byte to receive
- UxBRGH:L = value to achieve 250K baud rate
- UxRXPPS = code for desired input pin
- Selected input pin should be made a digital input by clearing the corresponding ANSEL bit
- ON =
1
Setting up a DMX Master (Controller) using the UART with Protocol Support
void UART_Initialize(){
UxCON0bits.MODE = 0b1010; //Select DMX mode
UxCON0bits.TXEN = 0; //Disable transmitter
UxCON0bits.RXEN = 1; //Enable receiver
UxCON2bits.RXPOL = 0; //Standard polarity, RX pin will idle high
UxCON2bits.STP = 0b10; //Recevie and verify 2 stop bits
//DMX data packet settings
UxP1 = 0x00; //Not used in DMX receiver
UxP2 = 0x10; //Address of first byte of interest
UxP3 = 0x20; //Address of last byte of interest
// Baud rate generator settings
UxCON0bits.UxBRGS = 1; //High speed baud generation
UxBRG = 0x3F; //Value for U1BRG for Fosc = 64MHz
//PPS settings for RX functionality (May vary device to device)
ANSELxbits.ANSELxy = 0; //Make Rxy a digital I/O
TRISxbits.TRISxy = 0; //Make Rxy an input
UxRXPPS = 0b010111; //Assign RX functionality to RC7
UxON = 0x01; //Turn on UART module
}