1.10.1 Auto-Baud Detect May Store Incorrect Count Value in the SPBRG Registers
When using automatic baud detection (ABDEN), on occasion, an incorrect count value can be stored at the end of the auto-baud detection in the SPBRGH:SPBRGL (SPBRG) registers. The SPBRG value may be off by several counts. This condition happens sporadically when the device clock frequency drifts to a frequency where the SPBRG value oscillates between two different values. The issue is present regardless of the baud rate Configuration bit settings.
Work around
When using auto-baud, it is good practice to always verify the obtained value of SPBRG, to ensure it remains within the application specifications. Two recommended methods are shown below.
For additional auto-baud information, see Technical Brief TB3069, "Use of Auto-Baud for Reception of LIN Serial Communications Devices: Mid-Range and Enhanced Mid-Range".
Method 1 - EUSART Auto-Baud Detect Work Around
#define SPBRG_16BIT *((*int) &SPBRG; // Define location for 16-bit SPBRG value const int DEFAULT_BAUD = 0x0067; // Default Auto-Baud value const int TOL = 0x05; // Baud Rate % tolerance const int MIN_BAUD = DEFAULT_BAUD - TOL; // Minimum Auto-Baud limit const int MAX_BAUD = DEFAULT_BAUD + TOL; // Maximum Auto-Baud limit ABDEN = 1; // Start Auto-Baud while(ABDEN); // Wait until Auto-Baud completes if((SPBRG_16BIT > MAX_BAUD) || (SPBRG_16BIT < MIN_BAUD)) { // Compare if value is within limits SPBRG_16BIT = DEFAULT_BAUD; // If out of spec, use DEFAULT_BAUD } // If in spec, continue using the // Auto-Baud value in SPBRG
0x67. The minimum and maximum
allowed values can be calculated based on the application. In this example, a ±5%
tolerance is required, so tolerance is 0x67 * 5% =
0x05.Method 2 - EUSART Auto-Baud Detect Work Around
#define SPBRG_16BIT *((*int)&SPBRG; // Define location for 16-bit SPBRG value const int DEFAULT_BAUD = 0x0067; // Default Auto-Baud value const int TOL = 0x05; // Baud rate % tolerance const int MIN_BAUD = DEFAULT_BAUD - TOL; // Minimum Auto-Baud limit const int MAX_BAUD = DEFAULT_BAUD + TOL; // Maximum Auto-Baud limit int Average_Baud; // Define Average_Baud variable int Integrator; // Define Integrator variable Average_Baud = DEFAULT_BAUD; // Set initial average baud rate Integrator = DEFAULT_BAUD * 15; // The running 16 count average ABDEN = 1; // Start Auto-Baud while(ABDEN); // Wait until Auto-Baud completes Integrator+ = SPGRB_16BIT; Average_Baud = Integrator/16; if((SPBRG_16BIT > MAX_BAUD) || (SPBRG_16BIT < MIN_BAUD)) { // Check if value is within limits SPBRG_16BIT = Average_Baud; // If out of spec, use previous average } else // If in spec, calculate the running { // average but continue using the Integrator+ = SPBRG_16BIT; // Auto-Baud value in SPBRG Average_Baud = Integrator/16; Integrator- = Average_Baud; }
0x67 *
5% = 0x05.Affected Silicon Revisions
| A2 | A3 | A5 | A6 | A7 | A8 | A9 | |
| X | X | X | X | X |