12.1.1 Connecting
To run the test, the test adapter and cable must be connected to the probe as shown in Figure 12-1. The edge connector mates directly onto the Mictor38 socket on the test adapter. Press firmly to ensure a good connection. The male part of the test adapter cable is connected to the probe. Note that although the hole for the cable is keyed so that the connector will only insert fully in the correct orientation, it is still possible to insert it halfway if using the incorrect orientation. The female part of the cable mates with the pin-header on the test adapter. Make sure this is mated correctly.