2.6.1.4 Functions

  • void BL_MemoryUnlockKeysInit (key_structure_t keys)

    Wrapper to the NVM Set Key function, which assigns the user-defined key values for write operations in the NVM.

  • void BL_MemoryUnlockKeysClear (void)

    Clears all the unlock keys once the bootloader core firmware completes the memory operations requiring them.

  • bl_mem_result_t BL_EEPROMRead (eeprom_address_t address, eeprom_data_t *buffer, size_t length)

    Wrapper to the NVM Read EEPROM function, which reads multiple bytes from the desired address in EEPROM.

  • bl_mem_result_t BL_EEPROMWrite (eeprom_address_t address, eeprom_data_t *buffer, size_t length)

    Wrapper to the NVM Write EEPROM function, which writes multiple bytes to the desired address in EEPROM.

  • bl_mem_result_t BL_FlashRead (flash_address_t address, flash_data_t *buffer, size_t length)

    Wrapper to the NVM Read Flash function, which reads multiple bytes from the desired address in the program Flash.

  • bl_mem_result_t BL_FlashWrite (flash_address_t address, flash_data_t *buffer, size_t length)

    Wrapper to the NVM Write Flash function, which writes multiple bytes to the desired address in the program Flash.

  • bl_mem_result_t BL_FlashCopy (flash_address_t srcAddress, flash_address_t destAddress, size_t length)

    Helper function to enable the direct copying of one Flash area to another.