2 Overview
The ZCD detects when an alternating voltage crosses through a threshold voltage level near ground potential. The threshold is the zero-cross reference voltage, ZCPINV. The connection from the ZCD input pin (ZCIN) to the alternating voltage must be made through a series current-limiting resistor (RSERIES). The ZCD applies either a current source or current sink to the ZCD input pin to maintain a constant voltage on the pin, thereby preventing the pin voltage from forward biasing the electrostatic discharge (ESD) protection diodes in the device.
When the applied voltage is greater than the reference voltage, the ZCD sinks current. When the applied voltage is less than the reference voltage, the ZCD sources current, thus allowing connection to high voltages without a resistance divider, and only through a series resistance.
The ZCD can be used when monitoring an alternating waveform for, but not limited to, the following purposes:
- Period measurement
- Accurate long-term time measurement
- Dimmer phase-delayed drive
- Low-EMI cycle switching
The ZCD requires a current-limiting resistor in series (RSERIES)
with the external voltage source. If the peak amplitude (VPEAK) of the
external voltage source is expected to be stable, the resistor value must be chosen such
that a 300 μA resistor current results in a voltage drop equal to the expected peak
voltage. The power rating of the resistor must be at least the mean square voltage
divided by the resistor value. The STATE bit in the ZCDn.STATUS register indicates
whether the input signal is above or below the reference voltage, ZCPINV. By
default, the STATE bit is ‘1’ when the input signal is above the
reference voltage and ‘0’ when the input signal is below the reference
voltage. The polarity of the STATE bit can be reversed by writing the INVERT bit to
‘1’ in the ZCDn.CTRLA register. The INVERT bit will also affect the
ZCD interrupt polarity.
The actual voltage at which the ZCD changes state is the zero-cross reference voltage. Because this reference voltage is slightly offset from the ground, the zero-cross event generated by the ZCD will occur either early or late with respect to the true zero-crossing. This offset time can be compensated by adding a pull-up or pull-down biasing resistor to the ZCD input pin. A pull-up resistor is used when the external voltage source is referenced to ground, and a pull-down resistor is used when the voltage is referenced to VDD, as shown in Figure 2-1.
The following equations help calculate the external components value:
In Idle sleep mode, the ZCD will continue to operate as normal.
In Standby sleep mode, the ZCD is disabled by default. If the Run in Standby
(RUNSTDBY) bit in the Control A (ZCDn.CTRLA) register is written to
‘1’, the ZCD will continue to operate as normal with interrupt
generation, event generation, and ZCD output on pin even if CLK_PER is not running in
Standby sleep mode. In Power-Down sleep mode, the ZCD is disabled, including its output
to pin.
The ZCD can generate the following events:
| Generator Name | Description | Event Type | Generator Clock Domain | Length of Event | |
|---|---|---|---|---|---|
| Peripheral | Event | ||||
| ZCDn | OUT | ZCD output level | Level | Asynchronous | Determined by the ZCD output level |
The ZCD has no event inputs.