Introduction
The Microchip IEEE® 802.15.4 PHY Library API provides an interface to the Application/MAC layer for utilizing the transceiver functionality of the PIC32CX-BZ2/WBZ45 devices. This document offers information on how to configure and enable the features of the API software. It includes a general description of each API, including their functionalities, syntax, responses, and examples. The API description defines the parameters, their types, valid/acceptable value ranges, default values (when available), and factory-programmed values (when applicable).