3 Mission Profile Examples
The values shown in the section SAM9X7 Series Lifetime Estimates are based on estimates for an always-on device (100% up time). However, all applications are not up 100% of the time and may switch from one operating point (TJ, VDD) to another. Such considerations must be taken into account when estimating lifetime.
To estimate a specific mission profile, use the following tables and examples.
The following table provides relevant definitions of terms.
| Symbol | Definitions |
|---|---|
| Generic | |
| TJ | Device junction temperature |
| VDD | VDDCORE voltage |
| User Mission Profile Data | |
| MP | User Mission Profile: a set of operating points (TJ,VDD) |
| PoHMP_TARGET | User Power-on Hours target with MP mission profile. This is the total time when the device is powered. |
| U% | Percentage of time spent in each MP operating point |
| PoH(TJ) | Power-on Hours spent at TJ. PoH (TJ) = PoHMP_TARGET x U% |
| Technological Data (see Figure 2-1 and Table 3-2) | |
| PoHQ(TJ,VDD) | Qualified equivalent hours at TJ, VDD. In particular, PoHQ(125°C,1.15V) = 2347 Hrs |
| DR(TJ) | Temperature-derating ratio at TJ : PoH[Q](TJ,VDD) = DR(TJ) x PoH[Q](125°C, VDD). See Table 3-2. |
| VAF |
Voltage Acceleration Factor PoH[Q](TJ, VDD) = VAF x PoH[Q](TJ, 1.15V)
|
| Calculated Quantities | |
| PoHMP(125°C, 1.15V) | Mission profile equivalent Power-on Hours at one point (125°C, 1.15V): PoH(125°C, 1.15V) = PoH(TJ) / (VAF.DR(TJ)) If this number exceeds PoHQ(125°C, 1.15V) then the mission profile MP is more demanding than the HTOL test. |
| PoHMP_EST |
Estimated Power-on Hours with given MP: PoHMP_EST = PoHMP_TARGET x PoHQ(125°C, 1.15V) / PoHMP(125°C, 1.15V) |
- In the above table, PoH[Q](TJ, VDD) means either PoH(TJ, VDD) or PoHQ(TJ, VDD).
Table 3-2, built from applicable product qualification, temperature and voltage aging acceleration values, lists the A, B, C and D operating points referred to in the example below.
| TJ | DR(TJ) | Mission Profile Example |
|---|---|---|
| TJ°C < 25°C | 938 | |
| 30 | 598 | A |
| 35 | 387 | |
| 40 | 254 | |
| 45 | 169 | |
| 50 | 114 | B |
| 55 | 77.7 | |
| 60 | 53.6 | |
| 65 | 37.3 | |
| 70 | 26.3 | C |
| 75 | 18.7 | |
| 80 | 13.5 | |
| 85 | 9.8 | |
| 90 | 7.1 | |
| 95 | 5.3 | |
| 100 | 3.9 | D |
| 105 | 2.9 | |
| 110 | 2.2 | |
| 115 | 1.7 | |
| 120 | 1.3 | |
| 125 | 1 |
- A target lifetime: PoHMP_TARGET,
- 4 operating points (VDD, TJ)
- A usage percentage in each operating point.
PoHMP_TARGET = 60000 Hrs
| MP | U% | PoH(TJ, VDD) | TJ °C | VDD (V) | DR(TJ) | VAF | PoH(125°C, 1.15V) | Comment |
|---|---|---|---|---|---|---|---|---|
| A | 25 | 15000 | 30 | 1.05 | 598 | 2.72 | 9 | 15000 / 598 / 2.72 = 9 |
| B | 25 | 15000 | 50 | 1.15 | 114 | 1.00 | 132 | 15000 / 114 / 1 = 132 |
| C | 25 | 15000 | 70 | 1.05 | 26.3 | 2.72 | 210 | 15000 / 26.3 / 2.72 = 210 |
| D | 25 | 15000 | 100 | 1.15 | 3.9 | 1.00 | 3823 | 15000 / 3.9 / 1 = 3823 |
| PoHMP(125°C, 1.15V) = | 4174 | |||||||
The PoH(125°C, 1.15V) column is computed for each line of the mission profile by derating PoH(TJ, VDD) with DR(TJ) and VAF (temperature and voltage derating). Computation results are then summed up into a single value.
- If the computed PoHMP(125°C, 1.15V) is greater than PoHQ(125°C, 1.15V), then the required PoHMP_TARGET exceeds the device lifetime emulated during the HTOL tests, as in this example. In such case, the mission profile must be reviewed.
- Conversely, if PoHMP(125°C, 1.15V) is less than PoHQ(125°C, 1.15V), then the mission profile MP is covered by the HTOL tests.
As explained above, PoHMP_TARGET = 60 kHrs cannot be reached with the example mission profile MP. However, it is interesting to estimate the Power-on Hours with such mission profile, PoHMP_EST. See applicable formula in Table 3-1 and its application in the following table.
| Result | Value in Hours | Comment |
|---|---|---|
| PoHMP_EST | 33700 | 60000 * 2347 / 4174 |