6.1 Device Addressing
Accessing the device requires an 8-bit device address byte following a Start condition to enable the device for a read or write operation. Since multiple client devices can reside on the serial bus, each client device must have its own unique address so the host can access each device independently.
The Most Significant four bits of the device address byte are referred to as the device
type identifier. The device type identifier ‘1010’ (Ah) is required in
bits 7‑4 of the device address byte (see Table 6‑1).
Following the 4-bit device type identifier is the hardware client address bit, A2. This bit
can be used to expand the address space by allowing up to two Serial EEPROM devices on the
same bus. The hardware client address bit must correlate with the voltage level on the
corresponding hardwired device address input pin A2. The A2 pin uses an internal
proprietary circuit that automatically biases the pin to a logic ‘0’ state
if the pin is allowed to float. In order to operate in a wide variety of application
environments, the pull‑down mechanism is intentionally designed to be somewhat strong. Once
the pin is biased above the CMOS input buffer's trip point (~0.5 x VCC), the pull‑down
mechanism disengages. Microchip recommends connecting the A2 pin to a known state whenever
possible.
Following the A2 hardware client address bit are A17 and A16 (bit 2 and bit 1 of the device address byte), which are the Most Significant bits of the memory array word address (see Table 6‑1).
The eighth bit (bit 0) of the device address byte is the Read/Write Select bit. A read operation is initiated if this bit is high, and a write operation is initiated if this bit is low.
Upon the successful comparison of the device address byte, the AT24CM02 will return an ACK. If a valid comparison is not made, the device will NACK.
| Package | Device Type Identifier | Hardware Client Address Bit | Most Significant Bits of the Word Address | R/W Select | ||||
|---|---|---|---|---|---|---|---|---|
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |
| All Packages | 1 | 0 | 1 | 0 | A2 | A17 | A16 | R/W |
For all operations except the current address read, two 8‑bit word address bytes must be transmitted to the device immediately following the device address byte. The word address bytes contain the lower 16 significant memory array address bits and are used to specify which byte location in the EEPROM to start reading or writing. See Table 6-2 and Table 6-3 to review their bit positions.
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|
| A15 | A14 | A13 | A12 | A11 | A10 | A9 | A8 |
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|
| A7 | A6 | A5 | A4 | A3 | A2 | A1 | A0 |