2 Overview
This section provides an overview of the MCHPRT3 tool setup and the components. Install the MCHPRT3_setup_v1.0.0.XXXX.exe tool. The MCHPRT3 tool installs by default in the C:\Microchip\ location.
The following table provides the MCHPRT3 tool package files:
| File Name | Description |
|---|---|
MCHPRT3.exe file | MCHPRT3 executable file |
MCHPRT3_CLI.exe file | MCHPRT3 CLI executable file |
uninstall.exe file | Uninstall the MCHPRT3 tool |
vc_redist.x86.exe file | Microsoft® Visual C++ Redistributable (x86) executable file |
The following table provides the PIC32CX-BZ3 package files:
| File Name | Description | |
|---|---|---|
| Examples>python3 folder | dll_wrapper folder | Contains conversion files between Python3 and the PIC32CX_BZ3.dll files |
| docs folder | Contains python3 example complied HTML help file | |
| gui_wrapper folder | Contains individual python3 Graphical User Interface (GUI) files | |
| gui_wrapper folder | Python3 example programming manager file | |
engine.py file | Python3 example file for the PIC32CX-BZ3 GUI | |
PIC32CX_BZ3_GUI.py file | Python3 example file for the PIC32CX-BZ3 GUI | |
version.py file | Version information | |
HEX file (.hex file) | Hardware Under Test (HUT) firmware version file | |
PIC32CX_BZ3.chm | PIC32CX-BZ3 complied HTML help file | |
PIC32CX_BZ3.dll file | PIC32CX-BZ3 dynamic link library file | |
PIC32CX_BZ3_CDECL.dll file | Default calling convention file for C and C++ programs | |
PIC32CX_BZ3_CLI.dll file | PIC32CX-BZ3 command line dynamic link library file | |
PIC32CX_BZ3_GUI.dll file | PIC32CX-BZ3 graphical user interface dynamic link library file | |
Release_note.txt | Tool release note file | |
Note: The MCHPRT3 tool works efficiently only with the HUT firmware version that is packaged with the package.