2.1 Private I3C/I2C Write Transactions using DMA
For a Private I3C/I2C Write transaction, it is recommended for the user to configure the DMA so that the data is transferred from the I3CxRXB register to a software buffer in the GPR space. The DMA can be triggered every time a data byte is received in the I3CxRXB register, which is available as a system level I3CxRXIF Receive Interrupt. It is not required to enable the system level I3CxRXIF interrupt for it to be used as a DMA trigger.
The DMA can be configured to transfer a set number of bytes to read from the I3CxRXB register. If it is possible that the controller might send less data bytes than that, the DMA can optionally be configured to be stopped when a TCOMPIF interrupt flag is observed. The TCOMPIF interrupt is available through the system level I3Cx General Interrupt. Although it is not required to enable the system level I3Cx interrupt to be used as a DMA trigger, the module level TCOMPIF interrupt must be enabled for this function.
| DMA1 Parameter | Setting | |
|---|---|---|
| SSA | Source Address | &I3CxRXB |
| SSZ | Source Size | 1 |
| SMR | Source Memory Region | SFR |
| SMODE | Source Address Mode | SPTR remains unchanged |
| DSA | Destination Address | Beginning of software receive buffer |
| DSZ | Destination Size | Number of bytes to read |
| DMODE | Destination Address Mode | DPTR is incremented |
| SIRQEN | Start Trigger Enable | Yes (enable when ready to receive data) |
| SIRQ | Start Trigger | I3CxRX (I3CxRXB is full) |
| SSTP | Source Counter Reload Stop | No – SIRQEN not cleared |
| DSTP | Destination Counter Reload Stop | Yes – SIRQEN is cleared when DCNT reloads |
| AIRQEN | Abort Trigger Enable | No (stops when SCNT reloads)(1) |
| AIRQ | Abort Trigger | N/A(1) |
|
Note:
| ||
How It Works:
- After SIRQEN is set, the DMA is
triggered as soon as data are available if the I3CxRXIF interrupt flag is set and
the content of the I3CxRXB register is transferred to the first address in the
software receive buffer. DPTR is incremented and now points to the following address
in the software receive buffer. Because SSZ =
1, the DMA stops after the first transfer. Since SSTP =0, SIRQEN remains set, and DMA waits for the next trigger. - When the data is available in I3CxRXB register again, the events in step 1 are repeated.
- After the desired number of bytes
have been transferred by the DMA (DSZ value), the DPTR reaches the end of the
allocated software buffer, and DCNT reloads. Since DSTP =
1, SIRQEN is cleared, and no further DMA transfers happen. - Optionally, if an abort trigger is configured using TCOMPIF, the DMA is aborted when the transaction is completed on the bus, regardless of the number of bytes transferred, which clears the SIRQEN bit.
Example Code for Private I3C/I2C Write Using DMA
// Example code for PIC18-Q20 device family uint8_t rxData[SWBUF_SIZE]; // Private Write DMA1 void DMA1_Initialize(void) { // Source and Destination settings DMASELECT = 0; // DMA Instance DMAnSSA = &I3C1RXB; // Source Address: Register in SFR space DMAnDSA = &rxData; // Destination Address: Variable in GPR space DMAnSSZ = 1; // Source Size: Source is only one register DMAnDSZ = SWBUF_SIZE; // Destination Size: Size of variable in GPR space DMAnSIRQ = 0x40; // Start Trigger: I3C1RX DMAnAIRQ = 0x00; // Abort Trigger: None DMAnCON1bits.SMODE = 0b00; // Source Mode: Pointer unchanged DMAnCON1bits.SSTP = 0; // Source Reload: No; SIRQEN not cleared DMAnCON1bits.SMR = 0b00; // Source Region: SFR/GPR space DMAnCON1bits.DMODE = 0b01; // Destination Mode: Pointer incremented DMAnCON1bits.DSTP = 1; // Destination Reload: Yes; SIRQEN is cleared DMAnCON0bits.SIRQEN = 0; // Start Trigger: Disabled (enable later when ready) DMAnCON0bits.AIRQEN = 0; // Abort Trigger: Disabled (stops when SCNT reloads) DMAnCON0bits.DGO = 0; // DMA Transaction: Do not start transaction yet // Clear interrupt flags PIR0bits.DMA1DCNTIF = 0; // Destination Count Interrupt PIR0bits.DMA1SCNTIF = 0; // Source Count Interrupt PIR0bits.DMA1AIF = 0; // Abort Interrupt PIR0bits.DMA1ORIF = 0; // Overrun Interrupt // Enable appropriate interrupts as needed PIE0bits.DMA1DCNTIE = 1; // Destination Count Interrupt (enabled) PIE0bits.DMA1SCNTIE = 0; // Source Count Interrupt PIE0bits.DMA1AIE = 0; // Abort Interrupt PIE0bits.DMA1ORIE = 0; // Overrun Interrupt //Enable DMA DMAnCON0bits.EN = 1; } void I3C1_ReceiveDataWithDMA(void) { // Clear RXB+RXFIFO if appropriate I3C1CON0bits.CLRRXB = 1; // Enable One-shot ACK (if ACKP = NACK by default) I3C1CON1bits.ACKPOS = 1; // Start DMA transfer with trigger DMASELECT = 0; DMAnCON0bits.SIRQEN = 1; } void __interrupt(irq(IRQ_DMA1DCNT)) DMA1_DCNT_ISR(void) { PIR0bits.DMA1DCNTIF = 0; // Code execution reaches here when DMA has completed transfer // Received data is now available for processing in rxData[] }