2.1 Device Block Diagrams

Device block diagrams will be made available for the Microchip web site to use on the Product Pages.

Device level block diagrams can be found in most data sheets. If the data sheet has a device level block diagram, select the image, right click and select Properties. Then set Image type to Device Block Diagram.

Remember: The applicable device(s) must be added to the publication properties.

When the WebHelp is published and set public, this block diagram will be available for the web site.

Figure 2-3. Device Block Diagram example

Sometimes a data sheet contains several devices and several block diagram, where each block diagram covers a sub set of the publication devices. All the block diagrams must have Image type to Device Block Diagram. Then, for each block diagram, set the appropriate devices in the image properties, in the Microchip specific fields.