6.3.1 Software Upload
Use this command to update the firmware controlling the switch.
Command Syntax:
firmware upgrade <url_file>Argument | Description | |
Parameter | <url_file> | Uniform Resource Locator (URL) is a specific character string that constitutes a reference to a resource. Syntax: <protocol>://[<username>[:<password>]@]<host>[:<port>][/<path>]/<file_name>. If the following special characters: space, ‘!’, ‘"’, ‘#’, ‘$’, ‘%’, ‘&’, ‘'’, ‘(‘, ‘)’, ‘*’, ‘+’, ‘,’, ‘/’, ‘:’, ‘;’, ‘<’, ‘=’, ‘>’, ‘?’, ‘@’, ‘[‘, ‘\’, ‘]’, ‘^’, ‘` ` `’, ‘{‘, ‘|’, ‘}’, ‘~’ need to be contained in the input URL string, they should be percent-encoded. A valid file name is a text string drawn from the alphabet (A–Za–z), digits (0–9), dot (`.`), hyphen (`-`), and underscore (`_`). The maximum length is 63 characters, and the hyphen must not be the first character. File names that contain only periods (`.`) are not allowed. |
Default | N.A | |
Mode | EXEC | |
Usage | Use this command to upload the firmware from TFTP Server to unit local file. | |
Example | Example 1: Upload firmware file test.mfi from TFTP Server. | |