1.5 FS SPI Flash Bootloader
This example application shows how to use the File System Bootloader Library to bootload an application from SPI Flash memory (SST26) to Internal Flash.
FS Serial Memory Bootloader Applications Block Diagram

Bootloader Application
This is a File System based bootloader application which resides from
- The starting location of the Boot flash memory region for PIC32MZ devices
- Uses a Custom linker script btl.ld to place it in Boot flash memory
- The starting location of the Boot flash memory region for PIC32MZ devices
It uses the Harmony 3 File System Framework to read the application binary (image.bin) stored in SPI Flash Memory and program it into Internal flash memory
It glows an LED once bootloader firmware is running
Trigger Methods
- It uses the On board Switch OR a GPIO pin as bootloader trigger pin to force enter the bootloader at reset of device
- It checks for bootloader request pattern (0x5048434D) from the starting 16 Bytes of RAM to force enter bootloader at reset of device
Programmer Application
This is a File system based SPI Flash programmer application which resides from
- The start of Program Flash memory for PIC32MZ devices
It will be loaded into internal flash memory from SPI Flash Memory by bootloader application
Uses the Virtual Com port of the device (EDBG port or External USB to UART converters) to send console messages
It Consist of three tasks
SDCARD_Tasks():
Receives the binary file image.bin to be copied into SPI Flash from SD Card
- As the application running in internal flash should have capability to copy new binary file to SPI Flash memory, we copy the programmer application binary itself in SPI Flash Memory
Prints copying status on UART console
SERIAL_MEM_Tasks():
Formats the SPI Flash memory to FAT File System if not formatted
Copies the binary file received by SDCARD_Tasks() to image.bin file in SPI Flash Memory. The copied image.bin from SPI Flash memory will be read by bootloader and programmed into internal flash
Prints messages on UART console
APP_MONITOR_Tasks():
Blinks an LED every 1 second
Prints messages on UART console
Uses On board Switch OR a GPIO pin to trigger bootloader once copying of image binary to SPI Flash memory is complete
Development Kits The following table provides links to documentation on how to build and run File System based SPI Flash bootloader on different development kits