1.5.1 PIC32 WFI32E Curiosity Board: Building and Running the File System based SPI Flash Bootloader applications
Downloading and building the application
To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions
Path of the application within the repository is apps/fs/spi/
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader/firmware/pic32mz_w1_curiosity.X | MPLABX Project for PIC32 WFI32E Curiosity Board |
Programmer application
| Project Name | Description |
|---|---|
| app_programmer/firmware/pic32mz_w1_curiosity.X | MPLABX Project for PIC32 WFI32E Curiosity Board |
Setting up PIC32 WFI32E Curiosity Board
To run the demo, the following additional hardware are required:
One micro SD Card
Connect IO1 Xplained Pro Extension Kit to the J203 XPRO header of PIC32 WFI32E Curiosity Board
On the GPIO Header (J207), connect U1RX (PIN 13) and U1TX (PIN 23) to TX and RX pin of any USB to UART converter (for eg: USB UART click board)
Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
Open the bootloader project bootloader/firmware/pic32mz_w1_curiosity.X in the IDE
Make sure that the app_programmer/firmware/pic32mz_w1_curiosity.X is added as a loadable project to bootloader application
- As the SPI Flash memory may not have any valid binary required by bootloader for the first time, Adding the app_programmer as loadable allows MPLAB X to create a unified hex file and program both these applications in their respective memory locations based on their linker script configurations

Open the Terminal application (Ex.:Tera Term) on the computer to get programmer application messages through UART once loaded
Configure the serial port settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and program the bootloader application using the IDE
Once programming is done bootloader starts execution and directly jumps to application space to run the programmer application
RED LED (D202) starts blinking indicating that the programmer application is running and you should see below output on the console

Open the programmer application project app_programmer/firmware/pic32mz_w1_curiosity.X in the IDE
Update app_programmer/firmware/src/app_monitor.c to update printf message from Serial Memory to SPI Flash Memory as below
printf("\r\n###### File System (SPI Flash Memory) Programmer Application Running ######\r\n");Clean and Build the project to generate the binary (Do not program the binary)
Copy the generated application binary file to a sdcard from the Host PC
- <harmony3_path>/bootloader_apps_serial_memory/apps/fs/spi/app_programmer/firmware/pic32mz_w1_curiosity.X/dist/pic32mz_w1_curiosity/production/pic32mz_w1_curiosity.X.production.bin
Rename the copied application binary file to image.bin
Insert the sdcard with the application binary image.bin in the micro-SD Card slot of the IO1 Xplained Pro Extension Kit
Following snapshot shows output of successfully copying the programmer application binary to SPI Flash Memory
RED LED (D202) should still be blinking

Remove the sdcard from the sdcard slot
Press and hold the Switch SW1/SW200 to trigger Bootloader from programmer application and you should see below output

Once Firmware Update is successful RED LED (D202) should start blinking indicating updated programmer application running and you should see below output on the console

Additional Steps (Optional)
To bootload any other application refer to Application Configurations
- Note that this application should have programming capabilities to SPI Flash Memory
Once done repeat the applicable steps mentioned in Running The Application