1.4.9 PIC32CX-BZ3 and WBZ35x Curiosity Board: Building and Running the QSPI Flash Bootloader applications
Downloading and building the application
To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions
Path of the application within the repository is apps/qspi_flash_bootloader/
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader/firmware/wbz351_curiosity.X | MPLABX Project for PIC32CX-BZ3 and WBZ35x Curiosity Board |
Programmer application
| Project Name | Description |
|---|---|
| app_programmer/firmware/wbz351_curiosity.X | MPLABX Project for PIC32CX-BZ3 and WBZ35x Curiosity Board |
Setting up
- Connect the Debug USB port on the board to the computer using a micro USB cable
Setting up the host script
- Refer to UART Host Script Help for setting up the uart_host.py utility used to send the application binary from host PC
There will be no reset command sent from host after programming by default.
Reboot command has to be sent separately only after successful programming to trigger bootloader from programmer application
Running the Application
Open the bootloader project *bootloader/firmware/wbz351_curiosity.X * in the IDE
Make sure that the *app_programmer/firmware/wbz351_curiosity.X * is added as a loadable project to bootloader application
- As the QSPI Flash memory may not have any valid binary required by bootloader for the first time, Adding the app_programmer as loadable allows MPLAB X to create a unified hex file and program both these applications in their respective memory locations based on their linker script configurations

Build and program the bootloader application using the IDE
Once programming is done bootloader starts execution and directly jumps to application space to run the programmer application
- RGB_LED_GREEN starts blinking every 500ms indicating that the programmer application is running
Open the programmer application project *app_programmer/firmware/wbz351_curiosity.X * in the IDE
Update app_programmer/firmware/src/app.c to reduce the LED blink duration from 500ms to 100ms as below
APP_TIMER_DelayMs(100);Clean and Build the project to generate the binary (Do not program the binary)
Run the uart_host.py from command prompt to program the updated programmer application binary in QSPI Flash memory
python <harmony3_path>/bootloader_apps_serial_memory/tools/uart_host.py -v -i <COM PORT> -d wbz351 -a 0x1002000 -f <harmony3_path>/bootloader_apps_serial_memory/apps/qspi_flash_bootloader/app_programmer/firmware/wbz351_curiosity.X/dist/wbz351_curiosity/production/wbz351_curiosity.X.production.binFollowing snapshot shows output of successfully programming the programmer application
- RGB_LED_GREEN should still be blinking every 500ms

To update the firmware, you can either:
Press USR_BTN_2 (SW3), then press RESET twice, OR
Run uart_host.py from the command prompt to send a Reboot command, then press NMCLR. This process updates the MetaData and triggers the Bootloader, which programs the updated binary from QSPI Flash to Internal Flash.
python <harmony3_path>/bootloader_apps_serial_memory/tools/uart_host.py -v -i -r

Once Firmware Update is successful RGB_GREEN_RED should start blinking every 100ms indicating updated programmer application running
- If there was any error you may need to power cycle the device to retry firmware upgrade
Update app_programmer/firmware/src/app.c to revert LED blink duration to 500ms from 100ms as below
APP_TIMER_DelayMs(500);Clean and Build the project to generate the binary (Do not program the binary)
Repeat Step 8-9.
- You should see RGB_LED (GREEN) still blinking every 100ms
Press the Switch USR_BTN_2 and then press RESET twice to Update MetaData and trigger Bootloader to program the updated binary from QSPI Flash to Internal Flash
Once Firmware Update is successful RGB_LED (GREEN) should start blinking every 500ms indicating updated programmer application running
- If there was any error you may need to power cycle the device to retry firmware upgrade
Additional Steps (Optional)
To bootload any other application refer to Application Configurations
- Note that this application should have programming capabilities to QSPI Flash Memory
Once done repeat the applicable steps mentioned in Running The Application