1 MPLAB® Harmony 3 Serial Memory Bootloader Application Examples

MPLAB® Harmony 3 is an extension of the MPLAB ecosystem for creating embedded firmware solutions for Microchip 32-bit SAM and PIC® microcontroller and microprocessor devices.

This repository contains the MPLAB Harmony 3 Serial Memory Bootloader application examples.

Bootloader Library

Refer to the Bootloader Library Help for understanding:

  • Bootloader framework
  • How the Bootloader library works
  • Bootloader library configurations
  • Bootloader memory layout

Bootloader Examples

The following applications are provided to demonstrate the Serial Memory bootloaders:

NameDescription
I2C EEPROM BootloaderThis example application shows how to use the Serial Memory Bootloader Library to bootload an application from I2C EEPROM (AT24) to Internal Flash
SPI EEPROM BootloaderThis example application shows how to use the Serial Memory Bootloader Library to bootload an application from SPI EEPROM (AT25) to Internal Flash
SPI Flash BootloaderThis example application shows how to use the Serial Memory Bootloader Library to bootload an application from SPI Flash memory (SST26) to Internal Flash
QSPI Flash BootloaderThis example application shows how to use the Serial Memory Bootloader Library to bootload an application from QSPI Flash memory (SST26) to Internal Flash
FS SPI Flash BootloaderThis example application shows how to use the File System Bootloader Library to bootload an application from SPI Flash memory (SST26) to Internal Flash
FS QSPI Flash BootloaderThis example application shows how to use the File System Bootloader Library to bootload an application from QSPI Flash memory (SST26) to Internal Flash