2.2.2 Extension Headers
Two extension headers needs to be soldered to the Xplained Mini board. This should be 10ˣ2 angled 100 mil headers, and they must be soldered to the bottom of the board. The optional single pin header should be soldered to the top of the board.
In the following figure, which pin that should be wired to which pin header is marked with the name of the pin. Note that even though the extension headers should be soldered to the bottom of the board, the drawings are from the top. To make the soldering process easier, it is recommended to solder the wires to the top of the board and to solder the wires before the extension headers.