12.3 Procedure to Visualize Touch Tune Data
Prerequisites to Enable Touch Tune Data:
- MPLAB Data Visualizer or MPLAB DV plug-in (if MPLABX IDE is already present) must be installed in the system.
- The UART to USB converter is required to stream the UART data from the MTCH1060 at a baud rate of 38400 to PC.
- The configuration files required to connect to DV can be downloaded from the MTCH1060 product page.
Procedure to connect DV:
- Open MPLAB Data Visualizer.
- Click on Connections, and
click the correct COM port. Enter the Baud rate in the COM
settings as shown in the following images.
- Select the Variable Streamer
tab and select the Auto-Configure option.
- In the Auto-Configure options,
select the correct folder path where the .ds files are available.
- From the Auto-Configure
drop-down, select the correct COM port to visualize the output.
- The MPLAB DV shows Tune Data from the
MTCH1060 as shown in the following image.