1.1.2.10 TCMECC_NoFixCallbackRegister
void TCMECC_NoFixCallbackRegister(TCMECC_CALLBACK callback, uintptr_t context)
Summary
Sets the pointer to the function (and it's context) to be called when the given TCMECC's UnFixable interrupt events occur.
Description
This function sets the pointer to a client function to be called "back" when the given TCMECC's interrupt events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called. The specified callback function will be called from the peripheral interrupt context.
Preconditions
TCMECC_Initialize must have been called for the associated TCMECC instance.
Parameters
callback - A pointer to a function with a calling signature defined by the TCMECC_CALLBACK data type. Setting this to NULL disables the callback feature.
contextHandle - A value (usually a pointer) passed (unused) into the function identified by the callback parameter.
Returns
None
Example
// Refer to the description of the TCMECC_CALLBACK data type for // example usage.