1.6 TCP/IP WEB NET Server NVM MPFS
The Web Net Server Non-volatile Memory (NVM) MPFS configuration creates a HTTP web server on a Microchip evaluation board. The Non-Volatile Memory (NVM) Microchip Proprietary File System (MPFS) is used for storing the web pages in the internal Flash.
This demonstration uses the HTTPNET server module that supports encrypted communication with NET_PRES layer and third-party TLS service provider (like wolfSSL).
Description
The TCP/IP WEB NET Server NVM MPFS application is based on MPLAB® Harmony 3 TCP/IP Stack.
The Harmony TCP/IP stack is a collection of different network protocols.
The source files of Harmony 3 TCP/IP stack is available here.
The demo is created with MPLAB X IDE and MCC plugin.
MCC Project Graph - TCP/IP WEB NET Server NVM MPFS
The following Project Graph shows the Harmony components included in the TCP/IP WEB NET Server NVM MPFS demo application.

wolfSSL component is added for secure connection which supports TLS.
wolfCrypt module enabled with MD5 and SHA authentication
FILE SYSTEM is added to select Memory module with Microchip file system (MPFS).
FreeRTOS component is required for RTOS application. For bare-metal (non-RTOS) FreeRTOS component should not be selected.
TCP/IP Configuration - TCP/IP WEB NET Server NVM MPFS
The TCP/IP modules enabled for the demo is shown in the TCP/IP Configuration Overview
More details of TCP/IP Configuration plugin is available here

The Application Layer modules enabled in the demo are as follows:
- Application Layer Modules
- ANNOUNCE to discover the Microchip devices within a local network.
- DHCP Client to discover the IPv4 address from the nearest DHCP Server.
- DNS Client provides DNS resolution capabilities to the stack.
- HTTPNET SERVER enables the target board to act as a Web Server for the secured port number 443.
- NBNS NetBIOS Name Service protocol associates host names with IP addresses. This assign of human-name host names to access boards on the same subnet.
- SMTP CLIENT let applications send e-mails to any recipient worldwide.
- SNTP Simple Network Time Protocol updates its internal time periodically using a pool of public global time servers.
Downloading and Building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
This content can also be downloaded using MCC content manager available as part of the MPLAB® X IDE.
Path of the application within the repository is apps\web_net_server_nvm_mpfs\ .
To build the application, refer to the following list of demo configurations and open the project using MPLAB X IDE.
| Project Name | Target Device | Development Board | Description |
|---|---|---|---|
| pic32wm_bz6_curiosity.X | PIC32WM_BZ6204 | PIC32-BZ6 Curiosity Board | TCP/IP WEB NET Server NVM MPFS Application - Bare Metal |
| pic32wm_bz6_curiosity_freertos.X | PIC32WM_BZ6204 | PIC32-BZ6 Curiosity Board | TCP/IP WEB NET Server NVM MPFS Application - FreeRTOS |
Hardware Setup- PIC32-BZ6 Curiosity Board
The target board for running the application is PIC32-BZ6 Curiosity Board.
This section provides essential hardware configuration of this target board to run TCP/IP applications.
Board Setup
- Default jumper setting of the board is shown above.
- Connect the USB Type-C cable between DEBUG USB port on the board and host PC.
- Establish a connection between the router/switch with the PIC32-BZ6 Curiosity Board through the RJ45 connector, using the Ethernet cable.
Running the Application
The HTTPNET Server module uses Microchip Proprietary File System (MPFS) to read web pages from the Non-Volatile Memory (NVM). The Non-Volatile Memory (NVM) is one of the memory media is used to store the web server pages.
- Open a terminal application on the host computer (like Hyper-terminal or Tera Term).
- Configure the terminal application for serial port “USB Serial Device”.
- Set baud rate as 115200 in the terminal application.
- Build and download the application project on the target board.
- Verify the TCP/IP Stack initialization console messages.

If DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board.
This will be printed on the console. Otherwise, the default static IP address will be assigned to the board.
By entering the command netinfo, the response is obtained as shown above.
Web Server Test
- Open a web browser (like Google Chrome, etc).
- Type the board URL in the address bar of web browser (for example, https://mchpboard_eth or https://<ip-address as shown in the console> ).
- The web browser display following web page

Application features are:
- Dynamic Variables and Real-time Hardware Control - Pressing Switches on target board toggles buttons on web page. Similarly, Clicking on LED symbol in web page can toggle LEDs on target board.
- Form Processing - Input can be handled from the client by the GET and POST methods.
- Authentication - Shows an example of the commonly used restricted access feature.
- Cookies - Shows an example of storing small text strings on the client side.
- Server Side Includes - An example of how SSI can be used to support dynamic content.
- File Uploads - Shows an example of a file upload using the POST method. The HTTP server can accepta user-defined MPFS/MPFS2 image file for web pages.
- Send E-mail - Shows simple SMTP POST methods
- Dynamic DNS - Exercises Dynamic DNS capabilities
- Network Configuration - The MAC address, host name, and IP address of the evaluation kit can be viewed in the Network Configuration page and some configurations can be updated
- MPFS Upload - A new set of web pages can be uploaded to the web server using this feature, which is accessed through https://mchpboard_eth/mpfsupload (or) https://<ip-address as shown in the console>/mpfsupload
Notes:
- For the LED and SWITCH demo functionality, configure the GPIOs connected to LEDs and Switches on target development board, through the Pin Configuration in MCC.
- The location of the MPFS image is fixed at the beginning of the Flash page specified by DRV_MEMORY_DEVICE_START_ADDRESS. The size of the MPFS upload is limited to DRV_MEMORY_DEVICE_MEDIA_SIZE in the demonstration. The HTTP File Upload functionality has to be enabled when the project is generated.