1.4 Interrupt Priority
Priority for the interrupts is determined by the interrupt vector address. An interrupt with lowest interrupt vector address has the highest priority. So reset has the highest priority followed by INT0, then INT1 and so on. If two interrupts occurs simultaneously, then the interrupt with higher priority is served first.