2.2 Enumeration and Detection
When the ATmega328PB Xplained Mini kit is connected to the PC, Windows® will enumerate the device and the install appropriate driver. If the driver installed successfully, mEDBG will be listed in the Device Manager as mEDBG Virtual COM port under Ports, as shown in the following screen-shots.