1 Harmony 3 Driver and System Service Application Examples for CEC173x Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
FAT File System using W25 Media | This application shows an example of using the FAT File System to access QMSPI based W25 flash media |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
USART Driver Asynchronous - UART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
USART Driver Synchronous - UART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |
W25 SPI Flash Read Write | This example application shows how to use the SPI driver to perform read and write operations on the on-board W25 Flash memory using the QMSPI peripheral library in SPI mode. |
W25 SQI Flash Driver - Flash Read Write in Quad IO Mode | This example application shows how to use the W25 SQI flash driver to perform block operations on the On-Board W25 Flash memory in Quad IO mode |