9.1 Program Memory Organization
PIC18 microcontrollers implement a 21-bit Program Counter, which is
         capable of addressing a 2 Mbyte program memory space. Accessing a location between the
         upper boundary of the physically implemented memory and the 2 Mbyte address will return all
            ‘0’s (a NOP instruction).
Refer to the following tables for device memory maps and code protection Configuration bits associated with the various sections of PFM.
The Reset vector address is at 000000h. The PIC18-Q41 devices feature a vectored interrupt controller
         with a dedicated interrupt vector table stored in the program memory. Refer to the “VIC
            - Vectored Interrupt Controller Module” chapter for more details.