6.3.1 Library Files
The compiler may include library files into the output per Figure 5-2.
By default, xc32-gcc will
search known locations under the compiler installation directory for library files that
are required during compilation.
Standard Libraries
The C standard libraries contain a standardized collection of functions, such as string, math and input/output routines. The range of these functions is described in the MPLAB® XC32 Language Tools Libraries Reference Manual for PIC32A MCU (DS-50003838).
User-Defined Libraries
You may create your own libraries. Libraries are useful for bundling and precompiling selected functions so that application file management is easier and application compilation times are shorter.
Libraries can be created manually using the compiler and the
librarian. To create files that may then be used as input to the 32-bit MCU librarian (xc32-ar), use the -c compiler option to stop
compilation before the linker stage. For information on using the librarian, see the
“MPLAB® XC32
Assembler, Linker and Utilities User’s Guide for PIC32A MCU” (DS-50003839).
Libraries should be called liblibrary.a and
can be added to the compiler command line by specifying its pathname
(-Ldir) and -llibrary. For
details on these options, see section 6.6.9 Options for Linking.
A simple example of adding the library libmyfns.a
to the command-line is:
xc32-gcc -mcpu=32AK1216GC41064 -lmyfns example.c -T
p32AK1216GC41064.gld
Library files specified on the command line are scanned first for unresolved symbols, so these files may redefine anything that is defined in the C standard libraries.
User-Defined Libraries Development
When creating your own libraries, follow the guidelines listed below.
Library and Supporting Files
No library file should contain a main() function,
nor settings for configuration bits or any other such data.
As with Standard C library functions, any functions contained in user-defined libraries should have a declaration added to a header file. It is common practice to create one or more header files that are packaged with the library file. These header files can then be included into source code when required.
ELF Libraries
MPLAB XC32 supports the object module format of ELF. ELF, combined with its debugging format DWARF, produces executables that contain a rich language for describing the artifacts of the executable program from a debugging perspective.
Should you wish to produce generic libraries that are ELF
compatible, we recommend that each library be named
liblibrary-elf.a. Naming the libraries in this way will
allow the linker to choose a correct library from the standard library inclusion
option. In other words, -llibrary will match first against
liblibrary.a followed by
liblibrary-elf.a.
Device Specific and Generic Libraries
If you would like to produce a library that will be compatible with a range of 32-bit MCU devices, you may need to include more than one copy of each object file in the library. This is perfectly acceptable, as long as each copy has a unique name. The linker will reject object files that do not match the characteristics of the user selected device.
Consider a simple library that contains one file (and one function)
name hello_world.c; you can guess at its use. The desire of this
function is to work on a range of devices, for example: PIC32AK1216GC41064 and PIC32AK6416GC41064. Compile
hello_world.c once for each device and combine them into one
library:
xc32-gcc -O1 -c hello_world.c -mcpu=32AK1216GC41064 -o hello_world.1.o
xc32-gcc -O1 -c hello_world.c -mcpu=32AK6416GC41064 -o hello_world.2.o
xc32-ar crv libhello_world-elf.a hello_world.1.o hello_world.2.o
This would produce a library that can be linked against any one of those devices.
xc32-gcc -O1 test.c -mcpu=32AK6416GC41064 -o test.exe -L. -lhello_world -T p32AK1216GC41064.gld
If a library is required to link against any device, the use of a
set of generic device names, listed in Readme_XC32.html or acquired directly from the tool using the
compiler option -mprint-devices, will produce object files that
will link against any device.