1.5.4.2 Using the Library

The PRIME Time Management service library is called by the PRIME PAL and the PRIME Library for time-related operations..

The following example illustrates how the Time Management service can be used.

Examples of PRIME Time Management Library Usage

uint8_t PAL_PLC_GetTimer(uint32_t *pTimer)
{
    *pTimer = SRV_TIME_MANAGEMENT_GetTimeUS();

    return (uint8_t)PAL_CFG_SUCCESS;
}

uint8_t PAL_PLC_GetTimerExtended(uint64_t *pTimerExtended)
{
    *pTimerExtended = SRV_TIME_MANAGEMENT_GetTimeUS64();

    return (uint8_t)PAL_CFG_SUCCESS;
}
static void lPAL_RF_DataCfmCb(DRV_RF215_TX_HANDLE txHandle,
                              DRV_RF215_TX_CONFIRM_OBJ *pCfmObj, uintptr_t ctxt)
{
    PAL_MSG_CONFIRM_DATA dataCfm;

    dataCfm.bufId = (uint8_t)ctxt;

    if (palRfData.rfCallbacks.dataConfirm != NULL)
    {
        dataCfm.txTime = SRV_TIME_MANAGEMENT_CountToUS(pCfmObj->timeIniCount);
        dataCfm.pch = (uint16_t)(palRfData.currentChannel | PRIME_PAL_RF_CHN_MASK);
        dataCfm.rmsCalc = 255;
        dataCfm.frameType = PAL_FRAME_TYPE_RF;

        switch(pCfmObj->txResult)
        {
            case RF215_TX_SUCCESS:
                dataCfm.result = PAL_TX_RESULT_SUCCESS;
                break;

            case RF215_TX_TIMEOUT:
                dataCfm.result = PAL_TX_RESULT_TIMEOUT;
                break;

            default:
                dataCfm.result = PAL_TX_RESULT_PHY_ERROR;
                break;
        }

        palRfData.rfCallbacks.dataConfirm(&dataCfm);
    }
}

uint8_t PAL_RF_DataRequest(PAL_MSG_REQUEST_DATA *pMessageData)
{
    DRV_RF215_TX_REQUEST_OBJ txReqObj;
    DRV_RF215_TX_HANDLE rfPhyTxReqHandle;
    uint8_t auxModScheme;

    txReqObj.psdu = pMessageData->pData;
    txReqObj.psduLen = pMessageData->dataLength;
    txReqObj.timeMode = (DRV_RF215_TX_TIME_MODE)pMessageData->timeMode;
    txReqObj.txPwrAtt = pMessageData->attLevel;
    auxModScheme = (uint8_t)(pMessageData->scheme) - (uint8_t)(PAL_SCHEME_RF) - 1U;
    txReqObj.modScheme = (DRV_RF215_PHY_MOD_SCHEME)(auxModScheme);
    txReqObj.timeCount = SRV_TIME_MANAGEMENT_USToCount(pMessageData->timeDelay);
    txReqObj.cancelByRx = false;
    txReqObj.ccaContentionWindow = pMessageData->numSenses;
    txReqObj.ccaMode = PHY_CCA_MODE_3;
    
    rfPhyTxReqHandle = DRV_RF215_TxRequest(palRfData.drvRfPhyHandle, &txReqObj, &txResult);

    (void)lPAL_RF_SetTxData(rfPhyTxReqHandle, pMessageData->pData, pMessageData->buffId);

    return ((uint8_t)PAL_TX_RESULT_PROCESS);
}