3.1.2.3 Acquisition Module APIs

touch_ret_t qtm_ptc_init_acquisition_module(qtm_acquisition_control_t* qtm_acq_control_ptr);

Description: Initializes the Acquisition module and PTC.

Parameter: qtm_acquisition_control_t*

Return: touch_ret_t

TypeDescription
qtm_acquisition_control_t*Pointer to acquisition control structure

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_ptc_qtlib_assign_signal_memory(uintx_t* qtm_signal_raw_data_ptr);

Description: Passes the pointer of an array. The unprocessed PTC output values for all the channels are stored in this array and used by the qtm_acquisition_process() API.

Parameter:

TypeDescription
uintx_t*Pointer to raw data array

where, x= 16, for 10-bit PTC/ADC devices

x =32, for 12-bit PTC/ADC devices

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_enable_sensor_node(qtm_acquisition_control_t* qtm_acq_control_ptr, uint16_t qtm_which_node_number);

Description: Enables a sensor node for measurement.

Parameter:

TypeDescription
qtm_acquisition_control_t*Acquisition Module Control Pointer
uint16_tNode (channel) number

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_calibrate_sensor_node(qtm_acquisition_control_t* qtm_acq_control_ptr, uint16_t which_node_number);

Description: Configures the sensor for calibration. On the next measurement, the calibration process for this sensor will be started.

Parameter:

TypeDescription
ptc_seq_acq_settings*Acquisition module control pointer
uint16_tNode (channel) number

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_ptc_start_measurement_seq(qtm_acquisition_control_t* qtm_acq_control_pointer, void (*measure_complete_callback) (void));

Description: Loads touch configurations for the first channel and starts the measurement. Subsequent channels will be configured in the PTC interrupt until all channels are measured. When measurement on all channel is completed, the callback function passed on this API will be called.

Parameter:

TypeDescription
qtm_acquisition_control_t*Acquisition module control pointer
void(*measure_complete_callback)(void)Measure complete callback function pointer

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_acquisition_process(void);

Description: Processes the acquired values (signal) resulting from calling the qtm_ptc_start_measurement_seq() API. This function must be called after the callback function, passed to qtm_ptc_start_measurement_seq(), is called by library.

Parameter: None.

Return: touch_ret_t

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_autoscan_sensor_node(qtm_auto_scan_config_t* qtm_auto_scan_config_ptr, void (*auto_scan_callback)(void));

Description: Configures the PTC to start measurement using Event System on a single node configured in qtm_auto_scan_config_ptr. When a touch is detected on the auto-scan sensor, auto_scan_callback() will be called.

Parameter:

TypeDescription
qtm_auto_scan_config_t*Pointer to the auto scan configuration structure
void(*auto_scan_callback)(void)Auto-scan wake-up callback function pointer

Return:

TypeDescription
touch_ret_tTouch library return status

touch_ret_t qtm_autoscan_node_cancel(void)

Description: Cancels Event System based measurement.

Parameter: None.

Return:

TypeDescription
touch_ret_tTouch library return status

void qtm_ptc_de_init(void)

Description: Clears PTC registers and sets the library state to TOUCH_STATE_NULL. The library can only after a proper initialization after calling this API.

Parameter: None.

Return: None.

uint16_t qtm_DEVICE_FAMILY_acq_module_get_id(void)

Description: Returns the module ID.

Parameter: None.

Return:

TypeDescription
uint16_tModule ID

uint8_t qtm_DEVICE_FAMILY_acq_module_get_version(void);

Description: Returns the module firmware version.

Parameter: None.

Return:

TypeDescription
uint8_tModule version

void qtm_ptc_clear_interrupt(void);

Description: Clears the End-of-Conversion (EoC) or Window comparator interrupt flags.

Parameter: None.

Return: None.

void qtm_DEVICE_FAMILY_ptc_handler_eoc(void)

Description: Captures the measurement and starts the next channel measurement. If EOC occurred for last channel, call the callback passed in the qtm_ptc_start_measurement_seq() API.

Parameter: None.

Return: None.

void qtm_DEVICE_FAMILY_ptc_handler_wcomp(void)

Description: Captures the measurement and calls the callback passed in the qtm_autoscan_sensor_node() API.

Parameter: None.

Return: None.

uint8_t qtm_claim_adc(uint8_t is_forced_claim)*

Description: The application claim the ADC before initiating any ADC measurements. uint8_t qtm_claim_adc(uint8_t is_forced_claim) API.

Parameter:
TypeDescription
uint8_t is_forced_claim0Claim ADC if available to use
1Force ADC claim - Terminate any pending ADC measurements and release the ADC
Return:
TypeDescription
uint8_t0Fail to claim ADC
1Successfully claimed ADC

void qtm_release_adc(void) *

Description: Application release the ADC after completing the ADC measurement. void qtm_release_adc(void) API.

Parameter: None.

Return: None.

Note: * - May not be available for all devices.