3.1.2.1 Data Structures
The acquisition module implements all functionality required for making relative measurements of sensor capacitance. This is the only module uniquely built for an individual device, as it must access and control the pins used for touch sensor implementation.
As devices have different hardware features available, different configuration options are available on each device. For the most efficient use of system resources—ROM and RAM—different sensor configuration structures are required.
However, where the same variable name is used within the structure, the functionality controlled by that variable is identical. Any dependent function should utilize a reference to the variable, and NOT rely on a reference to the structure and pointer arithmetic.
Acquisition Group Configuration
A reference by a pointer to
&ptc_qtlib_acq_gen1.freq_option_select will always point to
the correct memory location, regardless of the device. However, any implementation
based on pointer arithmetic will require refactoring if the code is to be reused
from one device to another.
| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
num_sensor_nodes | 16-bit | 0 to 65535 | The number of sensor nodes configured in the group |
acq_sensor_type | 8-bit |
NODE_MUTUAL | Defines the measurement method applied to this group of nodes |
calib_option_select | 1 byte | Bits 3:0 Calibration type:
CAL_AUTO_TUNE_CSD* | The calibration type selects which parameter should be automatically tuned for optimal charge transfer |
Bits 7:4 Calibration target:
CAL_CHRG_5TAU | The calibration target applies a limit to the charge transfer loss allowed, where a higher setting of a target ensures a greater proportion of full charge is transferred | ||
freq_option_select | 1 byte |
FREQ_SEL_SPREAD |
FREQ_SEL_SPREAD varies this delay from 0 to 15 in a
sawtooth manner during the oversampling set. |
PTC_interrupt_priority** | 1 byte | 1 to 3 | Interrupt priority level for the PTC. Applicable for all Arm® Device’s except SAME5x. |
| 1 byte | 1 to 7 | Applicable for Arm® SAME5x | |
wakeup_exp* | 1 byte | 0 to15 | The Wake-up Exponent is the exponent for the power of two, which represents the wake-up count in PTC core clocks |
cc_calib_precision* | 1 byte | 0 to 255 | The acceptable deviation in the measured signal value from the midpoint during calibration. Precision ensures that the calibrated signal value falls within the range of the PTC Signal Mid Value ± Precision |
|
Note:
* - Not available on all devices. ** - Applicable for Arm® Cortex devices only. | |||
Node Configuration
Similarly, node configuration structures vary depending on which device is used.
- Number of X lines
- Number of Y lines
- Feature availability
| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
node_xmask |
1/2/4/8 bytes | Bit field | Set the bit(s) at location(s) corresponding to the X line number(s). Example: X0 only =
X0 and X2 =
One byte is used for devices with up to eight X lines. Two bytes, four bytes, eight bytes are used for devices up to 16, 32 and 46* X lines, respectively.Note: *Can
support up to 64 X lines. |
node_ymask |
1/2/4/8 bytes | Bit field | Set the bit(s) at location(s) corresponding to Y line number(s). Example: Y5 only =
Y1, Y2 and Y7 =
One byte is used for devices with up to eight Y lines Two bytes, four bytes, eight bytes are used for devices up to 16, 32, and 46* Y lines, respectively.Note: *Can support up
to 64 Y lines. |
node_csd* | 1 byte | 0 to 255 |
The number of delay cycles to ensure charging of sensor node capacitance. Applicable for the AVR® ATmega324PB, ATmega328PB, Arm® SAML10/L11/L22, SAMC20/C21, PIC32CM_LE/LS, PIC32CK_SG/GC , PIC32CMPL 10 family only. |
| 1 byte | 0 o 31 | Applicable for the AVR® ATtiny family only | |
| 1 byte | 0 to 63 | Applicable for the ARM® SAMD51/E51/E53/E54 family only | |
| 1 byte | 0 to 127 | Applicable for the AVR® DA family only | |
node_rsel_prsc | 1 byte | Bits 7:4 = RSEL
RSEL_VAL_200* |
Internal Y line series resistor selection. * May not be available for all devices. |
|
Bits 3:0 = PRSC
|
Clock Prescaler The acquisition clock is derived and scaled from CPU clock for AVR® devices. * May not be available for all devices. | ||
node_gain | 1 byte | Bits 7:4 = Analog Gain
GAIN_16 | Analog Gain Setting Integration capacitor adjusted to control integrator gain |
Bits 3:0 = Digital Gain
GAIN_16 |
Digital Gain Setting The accumulated sum is scaled to digital gain | ||
node_oversampling | 1 byte |
FILTER_LEVEL_1024* |
The number of samples to accumulate for each measurement. Note: Oversampling must be configured to be
greater than or equal to digital gain for correct
operation.
|
|
Note: * - Not
available on all devices.
| |||
qtm_cvd_acq_dspic33ck_device_config_t| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
clk_src | 1 byte |
| Selects the ADC clock source |
clk_freq | 4 byte | Clock frequency based on the
clk_src selection | Frequency (Hz) of the clock source selected for touch timing |
ext_clk_freq | 4 byte | External clock frequency | External clock frequency (Hz) when using primary Oscillator with PLL |
device_id | 1 byte |
| Device selection |
qtm_acq_pic32xx_xx_device_config_t*| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
adc_interrupt_priority | 1 byte | 1 to 3 | Interrupt priority level for the ADC/PTC. |
adc_timebase | 1 byte | Based on the Clock frequency selection | The ADC timebase is a configurable parameter that defines the number of CLK_APB cycles corresponding to at least one microsecond (i.e. CLK_APB*0.000001). This setting ensures accurate internal timing for the ADC, independent of the ADC clock frequency, and is used to manage internal delays such as start-up times. If the CLK_APB clock frequency is modified and a new value is written to the TIMEBASE register, all timing counters will be reset. |
adc_pump_enable | 1 byte | Enable/Disable | The ADC voltage pump is an internal feature that must be managed depending on the operating conditions. Must be disabled when operating PTC above 4.5V, as leakage can affect PTC performance |
adc_prescaler | 1 byte |
x= 2,3,4,5,….….29,30,31,32 |
ADC Clock Prescaler The ADC acquisition clock is derived and scaled from CPU clock . |