3.1.4.4 Frequency Hop AutoTune API

touch_ret_t qtm_freq_hop_autotune(qtm_freq_hop_autotune_control_t *qtm_freq_hop_autotune_control);

Description: Performs Frequency Hopping Autotune algorithm. Measure noise in the signal value and based on the noise level, change the frequency-set used for acquisition. Also, chose the next measurements frequency from the frequency-set and perform median filter on the signal value. Should be called after calling qtm_acquisition_process().

Parameter:

TypeDescription
qtm_freq_hop_autotune_control_t *Pointer to Frequency Hop Autotune Control Structure.

Return:

TypeDescription
touch_ret_tTouch Library Return Status

uint16_t qtm_get_freq_auto_module_id(void);

Description: Returns the module ID

Parameter: void

Return:

TypeDescription
uint16_tModule ID

uint8_t qtm_get_freq_auto_module_ver(void);

Description: Returns the module Firmware version

Parameter: void

Return:

TypeDescription
uint8_tModule Version