6.1.1 Module description
Contains API prototypes for the SRAM March C- Test.
Figure 1. Unified Modeling Language (UML) Interface Diagram for the SW_SRAM_MARCH_TEST_01 APIs, using the March C- algorithm:

Figure 2. UML Sequence Diagram for using the Start-Up and Periodic SW_SRAM_MARCH_TEST_01 APIs with the March C- Algorithm:

There is an alternative UML sequence diagram for using the start-up SW_SRAM_MARCH_TEST_01 API and the March C- function directly on a user-defined section of the data. The data backup and its restoration is handled by the user application.
Figure 3. Alternate UML Sequence Diagram

Note:
Microchip Technology Inc. has followed development methods required by Functional Safety Standards and performed extensive validation and static testing to ensure that the code operates as intended. Any modification to the code can invalidate the results of Microchip's validation and testing.