15.1 Interrupt Operation

The compiler incorporates features allowing interrupts to be fully handled from C or assembly code.

The 32-bit DSC dsPIC33A devices allow interrupts to be generated from many interrupt sources. Most sources have their own dedicated interrupt vector collated in an interrupt vector table (IVT). Each vector consists of an address at which is found the entry point of the interrupt service routine. Some of the interrupt table vector locations are for traps, which are non-maskable interrupts which deal with erroneous operation of the device, such as an address error.

The interrupt controller has the capability to relocate the interrupt vector table (IVT) using the IVTBASE register. The IVT can be relocated anywhere within Flash/RAM by defining IVT in a new location and modifying the IVTBASE register accordingly. Also, the IVT can be collapsed by configuring the IVTC bit within the IVTCREG register. While trap handlers remain unaffected by this setting, all peripheral interrupts are directed to a singular location that follows trap vectors. For details on IVT relocating/remapping and IVT collapsing, see your dsPIC33A device data sheet.

Interrupts have a priority associated with them. This can be independently adjusted for each interrupt source. When more than interrupt with the same priority are pending at the same time, the intrinsic priority, or natural order priority, of each source comes into play. The natural order priority is typically the same as the order of the interrupt vectors in the IVT.

Interrupt code is the name given to any code that executes as a result of an interrupt occurring. Interrupt code completes at the point where the corresponding return from interrupt instruction is executed.

This contrasts with main-line code which, for a freestanding application, is usually the main part of the program that executes after Reset.