4.1.4.2 CS_ReadParameter Function
C
void CS_ReadParameter(CS_MemoryItemId_t parameterId, void *memoryPtr);Description
Gets the value of the parameter specified by its ID and writes it to the provided address in memory
\ingroup cs_functions
The function reads the value of a ConfigServer parameter specified by its ID. A parameter ID is a constant which name can be obtained by adding "_ID" suffix to the name of the parameter. For example, the identifier of the CS_NWK_PANID parameter is CS_NWK_PANID_ID.
The function copies the value to the location in memory specified by the second argument.
For example, reading the extended address of the device is performed this way:
ExtAddr_t ownExtAddr; CS_ReadParameter(CS_UID_ID, &ownExtAddr);
Parameters
| Param | Description |
|---|---|
| parameterId | the ID of the parameter to be read |
| memoryPtr | a pointer to which the parameter's value is written |
Returns
None