3.3.2 AES Engine
AES engine can be used to encrypt/decrypt stream of bytes. With APIs provided by HAL, it is possible to perform CBC/ECB - encryption/decryption the APIs HAL_AES_EncryptReq() and inputs are explained below with example
void HAL_AES_EncryptReq(HAL_AES_EncryptReq_t *reqParams_s)
The following actions in the enum, can be performed with the above API
/** Defines HAL AES commands such as setkey, cbc encrypt, cbc decrypt etc */
typedef enum
{
SM_SET_KEY_COMMAND = 0,
SM_ECB_ENCRYPT_COMMAND,
SM_CBC_ENCRYPT_COMMAND,
SM_ECB_DECRYPT_COMMAND,
SM_CBC_DECRYPT_COMMAND,
} HAL_AesCmd_t;
1. To set the key in the AES engine before performing encryption/decryption
/* Declare a memory for Encrypt request*/
HAL_AES_EncryptReq_t appSetKeyReq;
/* define a callback after key is set*/
void setAesKeyConf(void)
{
..
}
appSetKeyReq.aesCmd = SM_SET_KEY_COMMAND;
appSetKeyReq.text = &key; // 16 bytes of key
appSetKeyReq.blockcount = 1; // 128-bit block
appSetKeyReq.encryptConf = setAesKeyConf;
HAL_AES_EncryptReq(&appSetKeyReq);
2. To perform ECB encryption after setting the key
/* Declare a memory for Encrypt request*/
HAL_AES_EncryptReq_t appEncryptReq;
/* define a callback after key is set*/
void aesEncryptConf(void)
{
// Action to be taken after the encryption is completed for a block
..
..
}
appEncryptReq.aesCmd = SM_ECB_ENCRYPT_COMMAND;
appEncryptReq.text = &text; // 16 bytes of text to encrypt
appEncryptReq.blockcount = 1; // 128-bit block
appEncryptReq.encryptConf = aesEncryptConf;
HAL_AES_EncryptReq(&appEncryptReq);