1.1.3 Calibration Range
To achieve better accuracy the calibration range can be narrowed. In other words, to obtain better accuracy more calibration points are needed.
In the previous discussion it was assumed that the ADC characteristic is approximately linear between the calibration points. This is not necessarily the case. The characteristic is often approximately piecewise linear before and after some temperature. Choosing the calibration points wisely could result in increased accuracy after the compensation step.