1.1.4.1 Configuration Options
Default configuration options window for bootloader is shown below

Enable Console option
By enabling this option, Information on bootloader activities will printed into console using SERCOM UART. By Default, this option is disabled. When this option is enabled, make sure to connect the UART dependency in the bootloader with the SERCOM UART.
ECC Public Key
By default, ECC Public key is 0xc2,0x81,0x8f,0xbb,0x28,0x61,0x47,0x8b,0xa2,0x53,0x37,0x79,0xd4,0x63,0x18,0x7c,0x8b,0x41,0x59,0xa9,0x5f,0x0b,0x6b,0x94,0x4e,0xb9,0x57,0xa1,0x03,0xfe,0x20,0xbf,0x2b,0xb8,0x14,0x2a,0x64,0xb5,0xae,0x4a,0x83,0x80,0xdd,0xe6,0xee,0x29,0x89,0xdd,0xa0,0x9a,0xc7,0xda,0x82,0xeb,0x56,0x62,0x90,0x5d,0x66,0xc5,0xbc,0x30,0x3c,0x84
User should be able to change this key by changing the text box.
Supported Authentication Methods
- None
- SHA-256
- ECDSA-256
By Default, all these three modes are enabled. If customer want to use a specific authentication alone for security aspect, they can choose that alone
Enable Bootloader UART DFU option
By enabling this option, UART DFU (Device Firmware Upgrade) functionality will be enabled in the bootloader. DFU can be used to upgrade firmware on a target device through serially (UART). By Default, this option is disabled. When this option is enabled, make sure to connect the UART dependency in the bootloader with the SERCOM UART.
- GPIO Trigger DFU Mode
- Timer Based Trigger DFU Mode
DFU : GPIO Trigger DFU Mode Default Configuration
GPIO Trigger DFU Mode
In this mode, DFU functionality is enabled when you hold the GPIO button and press reset button to put the bootloader into the DFU mode.
Use GPIO Port and Pin option to change the port and pin based on the board . With PIC32CXBZ2 Curiosity board, GPIO PB4 is used as user button. The above default settings are based on this. User can change if different board is used
Timer based Trigger DFU Mode
In order to use timer-based trigger DFU Mode where bootloader will be in DFU Mode for the defined amount of time before jumping to the application, select the DFU mode to Timer Based Trigger. Change the DFU wait time if needed. DFU wait time is the time (in milliseconds) where the bootloader will be in DFU mode before jumping to the application.