"sxops" interface to finalise acceleration requests
and get the output operands
@file
SXOPS_IMPL_HEADER_FILE Macro
C
#define SXOPS_IMPL_HEADER_FILE
/ Copyright (c) 2018-2020 Silex Insight sa Copyright (c) 2018-2020 Beerten Engineering scs SPDX-License-Identifier: BSD-3-Clause
Make sure the application is compatible with SilexPK API version **/
SX_PK_API_ASSERT_COMPATIBLE(1, 0);
Finish an operation with one result operands
Write the single result in the result operand and release the reserved resources.
@pre The operation on the accelerator must be finished before calling this function.
Parameters
pkhw The acceleration request where an operation with 1 output operands has finished
Parameters
result Result operand of a single output operand operation static inline void sx_async_finish_single(sx_pk_accel pkhw, sx_op result) { const char outputs = SX_PK_GET_OUTPUT_OPS(pkhw); const int opsz = SX_PK_GET_OPSIZE(pkhw); SX_PK_MEM2OP(outputs, opsz, result); SX_PK_RELEASE_REQ(pkhw); }
Finish an operation with two result operands
Write the two results in the result operand and release the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
pkhw The acceleration request where the operation with 2 output operands has finished
Parameters
r1 First result operand of the operation
Parameters
r2 Second result operand of the operation static inline void sx_async_finish_pair(sx_pk_accel pkhw, sx_op r1, sx_op r2) { const char outputs = SX_PK_GET_OUTPUT_OPS(pkhw); const int opsz = SX_PK_GET_OPSIZE(pkhw); SX_PK_MEM2OP(outputs, opsz, r1); SX_PK_MEM2OP(outputs, opsz, r2); SX_PK_RELEASE_REQ(pkhw); }
Finish an operation with four result operands
Write the four results in the result operand buffers and release the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
pkhw The acceleration request where the operation with 4 resulting operands has finished
Parameters
r1 First result operand of the operation
Parameters
r2 Second result operand of the operation
Parameters
r3 Third result operand of the operation
Parameters
r4 Fourth result operand of the operation static inline void sx_async_finish_quad(sx_pk_accel pkhw, sx_op r1, sx_op r2, sx_op r3, sx_op r4) { const char outputs = SX_PK_GET_OUTPUT_OPS(pkhw); const int opsz = SX_PK_GET_OPSIZE(pkhw); SX_PK_MEM2OP(outputs, opsz, r1); SX_PK_MEM2OP(outputs, opsz, r2); SX_PK_MEM2OP(outputs, opsz, r3); SX_PK_MEM2OP(outputs, opsz, r4); SX_PK_RELEASE_REQ(pkhw); }
Write results in the result operand buffer and release the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
pkhw The acceleration request where the operation with 'count' resulting operands has finished
Parameters
results Buffer of result operands of the operation
Parameters
count The number of result operands static inline void sx_async_finish_any(sx_pk_accel pkhw, sx_op results, int count) { const char outputs = SX_PK_GET_OUTPUT_OPS(pkhw); const int opsz = SX_PK_GET_OPSIZE(pkhw); for (int i=0; i < count; i++) SX_PK_MEM2OP(outputs, opsz, results); SX_PK_RELEASE_REQ(pkhw); }