The PIC18F04/05/14/56Q20 devices you have received conform functionally to the current device data sheet (DS40002570A), except for the anomalies described in this document.

The silicon issues discussed in the following pages are for silicon revisions with the Device and Revision IDs listed in the table below.

The errata described in this document will be addressed in future revisions of the PIC18F04/05/14/15Q20 silicon.

Note: This document summarizes all silicon errata issues from all revisions of silicon, previous as well as current.
Table . Silicon Device Identification
Part Number Device IDRevision ID
A0
PIC18F04Q200x7AE00xA000
PIC18F05Q200x7AA00xA000
PIC18F14Q200x7AC00xA000
PIC18F15Q200x7A800xA000
Important: Refer to the Device/Revision ID section in the current “PIC18FXXQ20 Family Programming Specification” (DS40002327) for more detailed information on Device Identification and Revision IDs for your specific device.
Table . Silicon Issue Summary
ModuleFeatureItem No.Issue SummaryAffected Revisions
A0
I3CError Detection and RecoveryTE4 Error Not Detected When Module Operates in I3C Mode TE4 error not detected when module operates in I3C modeX
Error Detection and RecoveryTE0/TE1 Error Detection Cannot be Turned Off in I2C Mode TE0/TE1 Error Detection cannot be turned off in I2C modeX
Error Detection and RecoveryTE0 Error Detection Does Not Take R/W Bit Into ConsiderationTE0 Error Detection does not take R/W bit into considerationX
In-Band Interrupt/Hot-JoinPassive Hot-Join/In-Band Interrupt May Cause Race Condition to HappenPassive Hot-Join/In-Band Interrupt may cause race condition to happenX
UTMRLevel-Triggered ERS Start/Reset ConditionDead Zone Exists in Level-Triggered Start/Reset Condition When an ERS Signal Is Generated Due to an SFR AccessDead Zone Exists in Level-Triggered Start/Reset Condition When an ERS Signal Is Generated Due to an SFR AccessX
InterruptsInterrupts Do Not Work When Leaving Debug ModeInterrupts Do Not Work When Leaving Debug ModeX
Note: Only those issues indicated in the last column apply to the current silicon revision.