1.10 FLEXCOM TWI (I2C) EEPROM
This example application shows how to use the FLEXCOM module in TWI mode.
Description
This application configures the FLEXCOM peripheral in TWI mode to read and write data from an external EEPROM memory chip. Data is written to the EEPROM and then read back and compared. Successful comparison is indicated by turning on an LED.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/flexcom/flexcom_twi_eeprom/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
sam_9x75_curiosity.X | MPLABX project for SAM9X75 Curiosity Development Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
sam_9x75_curiosity.X | SAM9X75 Curiosity Development Board |
Setting Up SAM9X75 Curiosity Development Board
Additional hardware required:
- One EEPROM 3 Click board
-
Connect EEPROM 3 Click Board to MikroBus1 (J25) connector on the board
-
Connect the UART DEBUG J35 on board to the computer using a UART-FTDI cable (to enable debug com port)
-
Connect the USB port J2 on board to the computer using a micro USB cable (to power the board)
Running the Application
- Build the application using its IDE
- LED indicates the success or failure:
- LED is turned ON when the value read from the EEPROM matched with the written value
- LED is turned OFF when the value read from the EEPROM did not match with the written value
Board | LED Name |
---|---|
SAM9X75 Curiosity Development Board | RGB_LED (Green) |