3 Hardware Configuration
The hardware used for this example is based on the:
- AVR128DA48 Curiosity Nano (DM164151)
- Curiosity Nano Base for Click Boards (AC164162)
- mikroBUS™ POT click board (MIKRO-3402) or
- mikroBUS™ POT 2 click board (MIKROE-3325)
Two setups will be used for the use cases described in this document:
- The first configuration (Config A) uses a POT click, inserted in mikroBUS slot 1, connects AN1 to the PD3 (AIN3) pin of the AVR DA device.
- The second configuration (Config B) uses two POT clicks, inserted in mikroBUS slot 1 and slot 2. Slot 1 connects AN1 to the PD3 (AIN3) of the AVR DA device and slot 2 connects AN2 to PD4 (AIN4) pin of the AVR DA device.