1.3.1 Installing X2C Library
Pre-requisites
Install X2C Library
- Visit this link to download X2C v6.3 or above.
- Run the X2C Installer and follow the instructions
- At “Select Components” menu, select “Compact Installation with Microchip Support” and click “Next”
- Certain library files from X2C are required to be copied to your local MPLAB Harmony 3 X2C installation folder. X2C Installer can do this task, transparent to the user, as long as the user provides the local Harmony 3 installation path as shown below. This step would copy the required library files at <harmony 3 directory>\x2c_installer_files.
Note: This is a important step which adds Scilab/Xcos + X2C model
based development support in MPLAB Harmony 3 environment.
- Follow the rest of the self explanatory installation instructions to complete the installation of X2C.
- X2C Installer will also download and install the requisite version of Scilab/Xcos (if not already installed).