2.8 FVR Independent Gain Amplifiers
The following note is added to the section “Independent Gain Amplifiers”:
Important: Changing an analog peripheral's reference
voltage while the peripheral is enabled may cause undesirable behavior, including device
resets, oscillator drift, or reliability issues. If the analog peripheral's reference
voltage must be changed, disable the peripheral, update the reference voltage, and then
re-enable the peripheral. This applies to all analog peripherals, such as the ADC, DAC,
Comparator, etc..