7 Configure OSCHF to Run at 4 MHz with Incorrect Tuning Value
To better highlight the auto-tune feature, an incorrect value,
0x0F is placed in the OSCHFTUNE register. This increases the clock
frequency to a level above the error threshold. The following line of code loads the
OSCHFTUNE register with the desired value:
_PROTECTED_WRITE (CLKCTRL.OSCHFTUNE, 0x0F);
Figure 7-1 shows the CLKOUT
when 0xF is written into OSCHFTUNE register and Figure 7-2 displays the CLKOUT after the
auto-tune feature compensated the frequency drift.
At the end of the auto-tune procedure, the value in the tuning register is
0x01. This is different from the previous test, where the value was
0x00. As explained in the Overview section, this is normal behavior
when the error is smaller than what a single step would correct.