10.5.6 Other Linker Script Commands

There are several other linker script commands, which are described briefly:

ENTRY(symbol)

Specify symbol as the first instruction to execute in the program. The linker will record the address of this symbol in the output object file header. This does not affect the Reset instruction or vector, which must be generated in some other way. By convention, the XC-DSC linker scripts construct the correct instruction or vector at address 0x800000.

EXTERN(symbol symbol ...)

Force symbol to be entered in the output file as an undefined symbol. Doing this may, for example, trigger linking of additional modules from standard libraries. Several symbols may be listed for each EXTERN, and EXTERN may appear multiple times. This command has the same effect as the -u command line option.

FORCE_COMMON_ALLOCATION

This command has the same effect as the -d command line option: to make XC-DSC linker assign space to common symbols even if a relocatable output file is specified (-r).

NOCROSSREFS(section section ...)

This command may be used to tell XC-DSC linker to issue an error about any references among certain output sections. In certain types of programs, when one section is loaded into memory, another section will not be. Any direct references between the two sections would be errors.

The NOCROSSREFS command takes a list of output section names. If the linker detects any cross references between the sections, it reports an error and returns a non-zero exit status. The NOCROSSREFS command uses output section names, not input section names.

OUTPUT_ARCH(processor_name)

Specify a target processor for the link. This command has the same effect as the -p,--processor command line option. If both are specified, the command line option takes precedence. The processor name should appear in quotes; for example “33AK128MC106”.

OUTPUT_FORMAT(format_name)

The OUTPUT_FORMAT command names the object file format to use for the output file.

TARGET(bfdname)

The TARGET command names the object file format to use when reading input files. It affects subsequent INPUT and GROUP commands.