1.7 Fast Turn-OFF Break-Before-Make Switch
The turn on time of a typical driver is related to the input capacitance of the MOSFET it is driving. tON is 0.25 × 106 × (MOSFET CISS). Similarly, the turn OFF time of the driver is 106 × (MOSFET CISS).
In this situation, tOFF is greater than tON. For a system using multiple switches, however, there may be a problem since some switches will close before others open. Using the HT0440 as shown in Figure 1-8 will provide a solution to this problem and ensure that the correct switches open before others close. To achieve turn off time that is less than turn on time, a small depletion-mode MOSFET placed on the output of the HT0440 (as shown) will slow tON such that the circuit exhibits break-before-make switching.